Hi everyone. I'm trying to decide whether the TAS2552 will be suitable for my needs. There are various things that I haven't managed to extract from the data sheet. All help will be gratefully received!
What is the abs max differential Vpp out at the speaker terminals? I can see that the nominal boosted PVDD is 8.5V but I can't see how close to GND and PVDD the outputs will actually swing.
Can I drive AVDD and IOVDD from the same regulated rail or must they be separately regulated?
A related question; must AVDD and IOVDD be separately sequenced and if so, what is the minumum delay?
Can the TAS2552 be operated autonomously without a processor/I2C connection? If so what are the default gain and ILIM settings etc? The datasheet suggests thatthe I2C is needed for active current/AGC control but what if I don't need that? My application delivers a fixed amplitude modulated carrier which is simply switched on and off.
Is the ILIM a cycle by cycle limit in the boost converter or is it effectively a DC current limit feeding the output stage?
Thanks, Gareth