Hi,
I've constructed a TPA3116D2DAD PCB and have begun testing. It sounds great, but...:
I'm using Coilcraft MSS1210 10uH (10% sat @ 9.6A, 12mm x 12mmm x 10mm) chokes on the output together with 680nF PHE426 polypropolene caps. BTL mode with BD modulation.
The idle current (ready to play) is (no input signal applied):
48mA @ 12VDC input = 580mW
60mA @ 16VDC input = 970mW
86mA @ 24VDC input = 2W loss
I'm wondering if this is normal? The loss in idle is 2W at 24VDC supply? And the IC and chokes are getting hot (about 50-55C in idle). IC is cooled with small heatsink (2.4 cm x 3.0 cm x 1 mm alu) with 1mm thick gap pad (3W/K).
Without filter, the idle current consumption is about 40mA at 24VDC (within TI spec).
Looking forward to hear some input regarding this issue.