Hi all,
Would you mind if we ask TPA3140D2PWPEVM?
TPA3140D2PWPEVM's settings are followings;
-J10 : Open(Adjustment with R7(LIMTHRES))
-J8 : 32dB(Any XXdB setting, it occurs noise. )
-J9 : SLOW(FAST/NOMINAL setting, it occurs noise.)
-Power : DC13V max 5A
-Speker : 4ohm streo
-Input:1.5kHz sinwave(Any setting of XXkHz, it occurs noise.)
We have question about AGL function.
When the AGL function operates, we guess that the AGL fuction confirm the input level and adjust the gain level.
And then, it occurs noise.
So, when we use AGL function, is it common to occur noise?
Kind regards,
Hirotaka Matsumoto