Hi,
I am using Tpa3111d1 for driving a 4ohm speaker.
I want to control the output volume to the speaker from no output to maximum output. Right now I am using a pots at the input of the amplifier to suppress the audio input to the amplifier.
But even on using a pots of 1M ohm, output is still coming and speaker is driven.
I have kept the gain as 20dB and Plimit is very low (approx. 0V). Also the schematic is similar to the one given Evaluation board for Tpa3111d1.
Please suggest on how to achieve the same.
Regards
Abhijit