Is there an op amp that would be ideally suited for being used in a summing amplifier configuration for audio? I'm creating an audio mixer to mix two signals together.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The application will use a single supply with +3.3V power. The application is an audio mixer to mix an audio signal (not to be amplified) with an amplified microphone signal (using headphone amplifier).
Also I noticed an audio mixer circuit that was based on a transistor instead of an op amp...is there an advantage of using one method over the other?
Would there be an advantage to using an audio op amp like LME49721 instead of using a general purpose op amp?
I'm using the LME49726 audio op amp with a 3.3V supply and biasing the + input at VCC/2. I looked at the specs and found that the input common mode voltage range is from VSS+0.1 to VDD-1.6. With VCC/2 being 1.65V, this doesn't work well. The output of the op amp is connected to headphones (which can be as low as 10 ohms). Is there a better audio op amp solution for this?
Hi Ivan,
I'm using the LME49721, and it' gives a loud "pop" sound when it powers on. Is there a solution to eliminate this pop sound, or do I need to use an op amp with pop suppression? Do you have a recommendation?