SmartAMP support team,
I have 4 question about TAS2555 as follows,
[1] The pin assignment of ASI for multi-channel(ASIM) is not cleared at Function Block Diagram in page 18 of datasheet.
Please clarify the pin assignment of ASIM.
I found out other presentation material that the pin assignment was shown.
How to configure these pins using register?
[2] ASI2 controls both function of Echo Canceller and Noise Canceller. Is it possible to individually control ENABLE / DISABLE against each Canceller?
If possible, how to control or program register?
[3] What is the sound difference of SmartAMP / ROM mode1 / ROM mode2 to set in B0_P0_R34?
[4] And also, should all reister, B0_P0_R0 to B100_P0_R127, be programmed for SmartAMP mode?
Regards,
Tamio