Other Parts Discussed in Thread: TPA3128D2, TPA3244
I'm designing an amp for a portable speaker. 2 Ch X 2 Ohm load. Wattage handling of the driver is TBD, but expected up to 100W/ch, but 40=60W/ch may be the final for this application.
Options I'm considering
TPA3116D2 qty 2 in PBTL
TPA3128D2 qty 2 in PBTL
TPA3244 qty 1 in PBTL
Is there others that should be considered?
Why does the TPA3116D2 have a higher wattage rating over TPA3128D2 when the 3128 has lower RDSon?
If using TPA3116D2 "filter-free", are here concerns running at higher power?