Hi
I want to use the 3-Wire function of TAS5754M, But I can't use it well. So need you help.
if use TAS5754MEVM and use the Hybridflow 3 configuration, there is audio output.
But when we use ourself configuration, there is any audio output. I have try to give below two difference register value.
pls. give suggestion: which registers need to be configured and how to do ? thx
1)
Page0:
Reg 0x25 0x5A //Disable clock auto set;
Reg 0x0d 0x10 //PLL Reference clock is BCLK;
Reg 0x14 0x00 0x10 0x00 0x00 0x01 //PLL DIVIDER P, J ,D ,R
Reg 0x1b 0x01 0x0f 0x03 0x07 //DSP ,DAC,NCP, OSR CLOCK DIVIDER
2)
page 0
Reg 0x25 18
Reg 0x0D 10