Hi,
I wonder if there are any specific guidelines or recommendations for EMI-filter on the DC-power-supply-input for a design using TPA3221!
In my design I will use 2x TPA3221 and when I look at the EVM schematic there are only 3 caps on the DC-supply inputs! Is this sufficient from an EMC(EMI) point of view?
I will supply my design from an AC/DC adaptor with about 1.5m DC-cable.
Do I need to add for example a common mode choke at the DC-supply-input to my board?
Best regards
Markus