I have an application where I need the PWM output frequency to be <100kHz. I am able to operate the device in slave mode down to ~116.67kHz (700kHz input clock), but I am having difficulty going lower. I've increased the bootstrap caps for all 4 channels from 33nF to 100nF which seemed to work best. At 220nF, the lowest clock frequency is 900kHz.
Is there a way to safely get the device to work at ~100kHz PWM frequency?