Hi,
I have two questions related to bringing up a TAS5753MD board.
1) The TAS5753MD is responding to 7bit i2c address 0x2B (for example, I read back the correct device id from reg 1) confirmed with logic analyzer, and it is the only i2c device on the board. I note that this is a single right shift of 0x56 which makes me wonder if the datasheet is incorrectly listing 0x56 as the 7-bit address when it is really the "8-bit" address. If not, any ideas how this could have been reprogrammed? (I didn't intentionally try to change the address.)
2) Other than the registers specified in the startup sequence (osc trim and exit shutdown), what other registers are mandatory to configure to simply get playback functioning (or even 50% duty cycle switching for that matter)? By my reading only the master volume register 0x07 needs to be updated, am I missing anything?
thx