Hello Team ,please suggest a Speaker amps for below configuration
Vcc input =5V
- Stereo output
- 5 W/Ch into a 4Ω Load
- Two audio channel output ( As output should be stereo )
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team ,please suggest a Speaker amps for below configuration
Vcc input =5V
- Stereo output
- 5 W/Ch into a 4Ω Load
- Two audio channel output ( As output should be stereo )
Hi Shawn,
I study the datasheet of TPA3138D2 and it look ok but the things is that our system maximum voltage +5 volt. We are unable to use boost.
Is there any other amplifier that have 5W output per channel with 5V input? Amplifier with internal boost regulator??
We are also comfortable with class AB amplifier if it provide us 5W per channle with 5V input supply