hi sir,
im using LM2907 to convert frequency to voltage..i use optical encoder(sensor) to transfer signal to the LM2907 circuit. I connect my sensor to three-phase induction motor to count rpm and send the frequency(SIGNAL) to my f/v circuit. the circuit I used is from Ti's literature number SNAA088 (AN-162 LM2907 TACHOMETER/SPEED SWITCH BUILDING BLOCK APPLICATION) [page 5]...but I cnt get the output coltage..I also upload my circuit in breadboard...the output signal from my sensor also I upload here...some of circuit I try also I upload here...so anybody can help me to solve my problem..tq so much...
Details of my circuit :-
at pin 2 = 0.01microF (ceramic 103)
at pin 3 = 100k and 1microF (ceramic105)
at pin 4 =100k and 10microF (+/-)