Hi
I am trying to difference two voltages to measure the voltage drop across the device by using differece amplifier with help of LM358.
The switch is powerd with +24VDC and operating load of 20mA. The dropage while it gets ON is vaies from 3 to 8 mVDC.the gain of the amplifier is 10 and am expecting output voltage 30 to 80 mVdc. But unfortunately the voltage at output of the amplifier is 21VDC.
why its happening like this?
does the op- amp is capable to operate to differ the low voltage?
Please help to solve the issue.
Below shows the circuit which am testing.
I referring the below link.
Regards,
Nikhil