This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA230: BUS pin input impedance tolerance and negative voltage on IN- pin

Part Number: INA230


Hello,

I have two questions regarding the INA230:

  1. Can you provide a tolerance on the BUS pin input impedance?  The datasheet only lists 830k ohms with no min or max values.
  2. I am implementing low-side sensing and would like to connect the GND pin to the IN+ pin, which will result in a negative voltage at the IN- pin (about -12mV).  I know this is safe for the part per the Absolute Maximum Ratings, but will the differential voltage be read correctly by the ADC in this configuration?

Thanks,

Chris