Hi
This question is about Driven Right Leg (DRL). I found that the DC level of DRL signal, see below, from INA326 is not exactly 1/2V+. This makes the DRL circuit to be saturated.
Do you guys have any solution for improvement or avoid this."
Questions:
1. Can I use a capacitor with a large value, say 10uF, in between U4 and U5, to block the DC so that U4 will not be saturated? Will this make the DRL circuit have no 60Hz cancellation? I have tried it and it looked good. I could a 60Hz square wave at the output of U4.
2. How can I fine tune the the DRL circuit to make it has the best cancellation effect? I think I need to adjust the gain of U4 to achieve maximum cancellation.
Thank you very much
Xijun