Hello,
I'm trying to design an electrometer for detecting ions in a mass spectrometer. My first design used an OPA129U op-amp as shown in Figure 4 of its datasheet
The circuit works well, I confirmed the -10V/nA as described on the datasheet. However, I would like to make a second generation device with increased sensitivity as my first design was unable to see a signal from the relatively small numbers of ions I'm dealing with (hundreds to thousands of ions per scan)
One constraint is the electrometer pcb must be small enough to fit inside my vacuum chamber and as sensitive as possible. My other pcb was about 1.5" x 2" which should be relatively easy to accomplish. Are there any modifications I could make to the design or perhaps another more appropriate op-amp design that would give me more sensitivity and a lower detection limit?
thanks for your help!
Derek Wolfe
UNC Dept. of Chemistry