Hi,
We are using the SN74AVC16T245-Q1 level translator(16 IOs) to convert the 1.8V to 2.5V.
Q1. Will this device suitable to be used in GMII (Gigabit Ethernet interface)?
MAC side is 1.8V IO,the PHY chip is 2.5V IO. Will this level translator suits this application?
Q2. Will there be any skew among the 16 outputs?
The Tphl & Tplh are given some range values about 0.5 to 7.5 ns. I want to be clarified that the output1 to 16 will have same propagation delay values or it varies from port to port?
Please clarify us for the above two queries.
Thanks,
S.Sathiya Seelan
s.sathiya@mobiveil.com