Dear, All
The failsafe function operates at about 2.7 v to datasheet P8 Figure 2. of ISO7421 E-Q1 at the time of VCC1 falling, and outputting "High" to OUT is indicated.
Is a failsafe function canceled on the voltage same also at the time of the standup of VCC1?
Moreover, after reaching release voltage at the time of the standup of VCC1, if time until an actual failsafe function is canceled is known, please let me know.
Thanks, Masami M.