Hello
I have a question of UCC28070.
Please tell me about a noise measures method of the input electric current.
Please confirm an attached file about the details.
Best Regards,
Kei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I have a question of UCC28070.
Please tell me about a noise measures method of the input electric current.
Please confirm an attached file about the details.
Best Regards,
Kei
The inductor current is higher at lower input voltage and higher load current. Please measure the inductor current and check if there is inductor saturation during these conditions.
Hello Harmouch,
Thank you for your reply.
The inductor is not a saturated type.
Therefore there cannot be the thing that an inductance level suddenly falls at the time of high electric current.
- Inductor Current
RMS Current : 8Arms
Peak Current : 16A
Current of the noise : 11A
- Specifications of the inductor
RMS Current : 8Arms → 145uH
Peak Current : 16A → 85uH
Current of the noise : 11A →115uH
Would you tell me some causes that a noise happens?
Would you tell me some methods to reduce a noise?
I do not mind even a method thought about.
I'm sorry. I want an answer by 27th.
Sorry we had long weekend in US and was not able to answer by 27th. It is a current spikes and not noise. I can see it happens during zero crossing of the of the AC voltage. At zero crossing the rectified voltage is at its lowest value. The current demand is high. Make sure the input capacitor can deliver the current and has low impedance. You can try adding more ceramic capacitor.
I would like to see the following waveform:
1- rectified input voltage VIN
2- Inductor current
Hello Mahmoud,
Thank you for your support.
It is said that I cannot submit them from the OEM maker.
I inform it of an assumed cause by the following contents.
- It is thought that lack of adjustment of Rsyn.
- It is thought that adjustment frequency of CAOA and CAOB is too low.
- It is thought that RC filter of CSA and CSB is too big.
Best Regards,
Kei