It is not clear to me how to determine whether or not a particular part will meet the ESR requirements of the output capacitor for the TPS7B4250.
The ESR for ceramic capacitors that I have been reviewing for use with the TPS7B4250, do not have a single ESR value, rather, there is a graph showing ESR vs Frequency (typ. 100 Hz to 3 MHz (<self-resonance).
At what frequency(s) should the listed 0.001 to 20 Ohms required ESR of the capacitor be evaluated at?
I have searched this forum and found several questions regarding ESR and TI LDO regulators, but answers similar to “10 kHz to 100 kHz should be ok” and “that part looks good to use” did not provide a means of understanding how to determine the relevant ESR frequency(s) for TI LDO regulators if none is stated in the datasheet.
Thank you,
TonyS