Dear all,
This device has low INL=1LSB.
But I feel that this Gain error and Gain drift is big.
Gain error: 0.25%(MAX)→This is equal to 10 LSB because of 12 bit ADC.
Gain drift: 40ppm/℃(MAX)→This become to 0.4% at changing 100℃. This is equal to 16.4 LSB.
In this bad situation, the significant bit become 7~8 bit because of 26 total bit.
Is this device premised on correcting Gain error / Gain drift?
Best regards,