Hi,
The platform is TDA2XX, under SYS/BIOS.
The DCAN is in normal mode, only want to send data.
The registers were configured according to datasheet, but the DCAN could not send data.
By finding the value of the registers, I meet the following problems.
Question 1:
The TxRqst bit is set (TxRqst = 1), the NewData bit is set (NewData = 1). And the registers of IF1DATA/IF1DBTB has the data need to be send. But the value of the Message RAM (0x4ae3d0000 + offset) is 0x00000000, which means no data in the Message RAM.
According to the datasheet, when the bit of TxRqst and NewData are both set to one, the transmit begin. But there is no any data is sent out.
Question 2:
The Message Object (0x40) find the parity error. But I don't enable the function of parity check.
Question3:
Whether need to enable the function of Automatic Retransmission?? (Normal mode, only want to send data).
Question4:
Whether need to enable the function of Auto-Bus -On?? (Normal mode, only want to send data).
Hope to get some advice.
Ann