Hello,
Are there any EMI data of TPS40210-Q1?
Our cusotmer using the MAX16990 which has the Spread spectrum function.
We are promoting the TPS40210-Q1 to the customer but they can't change due to the TPS40210-Q1 doesn't have the Spread spectrum function.
If we can show the TPS40210-Q1 EMI performance which is better than MAX16990, they may consider to use our device.
Best Regards,
Ryuji Asaka