Hola,
We used TPS92630-Q1 in our new project design and have found one issue about that we cannot get the fault signal from the FAULT pin.
After analysis, we found the reason that why we cannot get the open load signal.
The problem is from DC20 and DC19 TVS diode.
If we put the TVS diode at the Iout path then we cannot get the fault signal active even we remove the LED module.
This may have the ESD protection issue, does TI have any suggestion for this?How do we detect LED works normally?
By the way, if we changed Vin to 12V then will it get the Iout voltage over 12V or it will be lower than 12V in maximum output current?
In addition, the TVS voltage of DC20 and DC19 and LED number and forward voltage were listed as below:
VISHAY (VESD05A1B-HD1-GS08) 6.8V TVS & LED is 3V forward voltage the number is one.