Hello,
I would want to interface a TSW1250EVM with AFE5804EVM in order to acquire and process data on a PC. It is specified that the TSW1250EVM is specifically designed for AFE5804EVM, but it is also stated on the page of the product that I should consider to use the new TSW1400EVM instead. Is this new device still compatible with AFE5804EVM or do I need to use the TSW1250EVM ?
I also need to process the data with Matlab. It is stated in the datasheet that it is possible with the TSW1200EVM, but is it possible as well with the TSW1250EVM ?
Thank you for your help.
Best regards,
Yorick