Hello all,
I am currently working on using MPU9150 with AFE4400SPO2EVM.
I noticed the footprint for MPU9150 on EVM and have soldered all the components and the chip related to it on the EVM. But I am not being able to communicate with the device.
I have a perfectly working code for I2C communication which works fine with MPU9150 and MSP430F5529.
But when I try to use the code on the EVM then it is not working.
I checked the clock cycle (SCL)on the MSP430 but it came out to be zero, also the SDA pin is always high.
Thus it assumes that the I2c is in busy state.
Can anyone help me on this?
also has anyone tested the MPU9150 on EVM or can anyone varify the schematics used in the EVM?