Hello,
I'm testing the AFE5401 EVM, but I'm having several difficulties.
The issue is that every time I power it on, it can enter into 1 of 3 different power states: 170 mA, 380 mA, or 560 mA (at 5V). I've tried a software reset with no change (I verified the software reset by writing to the register, reading the register to see that it was written, then call reset and recheck the original register, which had all bits low). When I put the hardware reset low it reduces the power draw by 170 mA from whichever state it is in.
I don't see any register that corresponds to switching between power states, which causes me some concern for our final designs. Additionally these power states affect the reliability of all aspects of the ADC, including adding a dc offset to the DCLK, and driving all output bits high.
Any help would be appreciated.
Farris