Hi all,
I am working with AFE5808 evm and TSW1400, I have programmed in Quartus II to receive ADC Differential LVDS data (320MHz) and route the data to SYNC1(J14),SYNC2(J15) on TSW1400 board. When I download my customized firmware in board, I have observed in oscilloscope the analog input channel of AFE is getting noisy (Note : nothing analog input is fed to AFE). But for the AFE5808_14b firmware no noise introduced at the AFE input.
Can somebody help me to solve this problem.
I having one doubt that what is the IO Standard and drive strength settings of the input pins of tsw board.
Thank you.
regards,
chandu.