Hi
I have downloaded the schematics from your website and have some questions related to the same:
1) DVCC_JTAG is coming to input pin of TPS2115ADRB and is coming from connector J1.But I am not getting from where it is being generated. Please clarify.
2) BQ2745 is the battery monitor IC. But the Vcc is connected to LDO_OUT_FG/BAT_DET which is further going to an interrupt based GPIO of MSP430. Can you please clarify the connection?
3) Vcc of BQ2745 needs a supply of 2.75V as per datasheet. Can you please tell me any where in the circuit 2.75V is being generated or it can be powered on by 3.3V itself?
4) What is the usage of multiplexer TPS2115ADRB? Because it is used to select two signals LDO_3v3 and DVCC_JTAG. Please clarify the requirement.
5) In power supply circuit what is the requirement of UC3833? Please describe.
Thanks
Arnab