Hi,
I have a CCA that uses a microcontroller (uC) to write/read registers in the AFE5808A, and am looking to see if I can use the same, unmodified uC code to work with an AFE5812. To make the AFE5812 "equivalent" to the AFE5808A, it appears I only need to disable the Demodulator in the AFE5812 by writing a '1' to register 22[0] (i.e. 0x16[0]). However, register 22[0] is reserved/unlisted for the AFE5808A; also, the AFE5808A data sheet says that "During register programming, all reserved/unlisted register bits need to be set as '0'".
My question is, will there be a problem if I write a '1' to register 22[0] on the AFE5808A?
Thanks,
Eric