My customer is seeing Vout levels above the levels that are listed in the data sheet when using the TLK2711-SP model. He is using pre-emphasis at 20%, but the simulation seems to be showing differential voltage levels of nearly 3V pp using the fast/strong model. It is even showing differential voltages of 2Vpp in the slow/weak mode. Can you verify if there is an issue with the model?
I have attached a picture of what the customer is using in the simulation.
Can you verify if this is an issue or not?
Thanks for your help with this!
Richard Elmquist