Hello
SN54LVC573A is 5-V tolerant tolerant input which means you can apply input of 5.0V having vcc of 3.3V. I'm confused with the output voltage range in 3-state which can be 5.5V. In my application, the input voltage is 5.0V when the latch is 3-state. Does it mean that in 3-state 5.0V can appear on the output pins of latch if the input voltage is 5.0V or it means that in 3-state output pins are also 5-v tolerant regardless of the input voltage?
Regards;