Hello,
I was wondering if there was a way to reset the chip or fix the impedance reading (voltage sense or the current output). Right now, I have the chip at 1.7 Ref voltage. It used to be able to read the voltage across a resistor of 20k Ohms, but currently it has been reading across a resistor of a 2k ohms as its max. I have double checked the connections and used the GUI to reset the chip, but it still seems to be unable to read a voltage across anything higher than 2k ohms.
Thanks.