I have noticed the circuit board layout in the datasheet. Is there a populated evaluation PCB available from your lab? It would be good if there is one.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have noticed the circuit board layout in the datasheet. Is there a populated evaluation PCB available from your lab? It would be good if there is one.
Cornelis,
Can I get your email to take this offline?
Yes you can have my email which is :cornelis_klein@yahoo.co.nz I am building an NMR application and have not had much luck with the front end. I have basic PCB manufacturing facilities and can not really handle more than 2 layers. Also when the size of the package is so small that the board processing is pushed to limits it gets hard. Because the layout for the TL5500 is on the datasheet I was wondering if there are ready made boards of that TI design. It would help me a great deal thank you.