Part Number: TPIC84000-Q1
Hi,
I am trying to wake up and configure the TPIC84134-Q1 via SPI commands. Therefore, I have several issues that need to be solved:
1 - Is there any master device or SPI conversor recommended for sendind the 64 bits command to the TPIC in an intuitive way? Something recommended by TI?
2 - How can I check if the device has woken up with the 0x9000000000000000 command?
3 - Following the recommendation design in the datasheet in Figure 8, both Out1 and Out2 are connected by the antenna. Therefore, should I configure both Outputs to transmit? Or just Out1?
Thank you so much in advance