Hi,
We are using the power meter feature of AFE7225 for monitoring the received power level in dBfs. We want to develop an algorithm which sets the RF gain before ADC with respect to the value read from AFE7225's power meter. If there is no signal, it shows "0" meaning that the signal level at ADC is <-15dBfs. For increasing the power that comes to ADC, we will decrease the attenuation level until the AFE7225 reads the power level -1dBfs (value = 15). However, when we increase the input power more after getting -1dBfs, we saw that there is a 10dB margin in -1dBfs level and later if we increase the power more, it turns to "0" value due to high level of the power.
If the read power from AFE is "0", we don't know why it is zero. It can stem from low level of signal level or huge level of signal level. If it is due to huge level signal level and if our algorithm says to increase the gain of the circuit by thinking there is a low level signal, maybe the device will be damaged due to high power level of the signal. Is there any way for solving this problem?
Regards,