This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300: AFE4300 How to Measure / Calculate Resistance and Reactance

Part Number: AFE4300

Reviewing all the available documentation and forum activity for the AFE4300, I don't see any information on how to directly measure or calculate the Resistance and the Reactance using the AFE4300.  As I understand it, the AFE4300 can measure Impedance using FWR at all frequencies and can also measure / calculate Phase Angle and Impedance at limited (8, 16, 32, 64, and 128 kHz) frequencies using IQ mode.

So how to measure Reactance and Resistance? Preferably at all frequencies as I have not come across any BIA formulas that use the IQ mode frequencies.  Most use 1, 5, 50, and 100 kHz.