Hello,
I am looking for a motor driver for an unusual application. I want to test the mechanical condition of a small turbine generator with a permanent magnet three-phase coil (thus a three phase PMSM, but used as a generator). For testing it I want to drive it as a motor with a simple test setup, utilising a sensorless motor driver. I was thinking of starting with the evaluation board for the new DRV11873. When the whole assembly is driven this way, I can determine its mechanical condition (mainly degree of friction of the bearings) by looking at the achieved RPM and consumed input current at a certain input voltage.
The challenge is that the turbine generator may have fairly high friction, specially at zero RPM, so it will need all the torque that such a sensorless motor driver can give, right from the start, to begin rotating at all.
To my understanding the typivcal driver configurations start with a controlled ramp until sufficient back EMF is available for the sensorless control mode. In my application such a ramp may need to be fairly slow, to overcome the startup friction.
For the DRV11873 I did not find any information about details of the startup algorithm however. Therefore my question, if this driver evaluation module would be suitable for my application, would the ramp likely be slow enough?
Thanks in advance.
HJWF