Hello,
My customer has a question about DRV11873.
[Q]
They want to use the device to control the motor at around 7200rpm,but the motor always stops at around 7200rpm.
It can control the motor at around 10000rpm.
I watched the following post.
DRV11873EVM - Motor stops over 9500rpm (http://e2e.ti.com/support/applications/motor_drivers/f/38/t/314799.aspx)
The result is as follows when I use the formula of mention for that post.
FG = RPM * PP / 60 = 7200 * 12 / 60 = 1440Hz > Maximum speed limit 950Hz@FS=1
Is this a problem of maximum speed limit control ?
Can DRV11873 control the motor at around 7200rpm ?
[Motor Information]
- Manufacture name : NIDEC Corporation
- Series : Smart_28S series (http://www.nidec.com/en-IN/product/motor/category/A010/B010/P0000014/)
- Rated Speed : around 7200rpm
(Product information of the URL describe rated speed with 9200rpm~, but rated speed of the customer's custom motor can operate around 7200rpm.)
- Pole Pair (PP) numbers : 12
Best Regards,
Hiroshi Katsunaga