I have 2 questions on DRV8711 datasheet.
1) I need to set 2.5 uS blank time. Which value should I program to BLANK register? In the BLANK register description there is range 1uS..5.12uS and values 0x00 - 0x32 are the same (1uS). According to this logic I need to program 0x7D for 2.5uS. But in this case 0xFF will correspond to 5.1 uS, not to 5.12 uS. Page 6 has another range for this timing (0.5..5.12 uS). I saw the same question here, but without any answer.
2) I am using DRV8711 in half-step mode. Based on datasheet, the home position for this mode is 45 degrees (when 2 windings are switched on at 71% level). But in reality after resetting and programming the IC only one winding is switched on at 100% level. Is there a mistake in PDF? What is real home position?
Thank you!