Hello,
I am trying to setup the DRV8308EVM for the first time. The included motor is wired as shown in the user guide and i'm supplying the board with 24V. The jumpers are in the positions shown in the user guide. When I connect the board to the computer/gui both the FAULTn and LOCKn indicators on the GUI are red. The led's on the board itself are off. When pressing enable nothing happens. If i hit the reset button, the motor turns on for a few seconds and seems to run normally but then the fault led turns on and the motor stops. FAULTn and LOCKn never turn green on the GUI.
Also if i try to adjust the duty cycle it just reverts back to 1%.
The settings i have on the GUI PWM mode tab are as follows.
Control mode: PWM from MSP430
Commutation: 120 deg
Advance: 30
Speed 1500
MOD120: 2048
HALLPOL: Inverted
Thanks in advance
Aaron