what is the maximum input PWM frequency can be used with DRV8301?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what is the maximum input PWM frequency can be used with DRV8301?
Hi Shashank,
The recommended maximum PWM frequency is 200kHz. This also depends on the gate drive current based on the FET charge.
Refer to section 8.2.2.1 for approximation the switching frequency.