Dear all,
Could you teach about definition of dead time and propagation delay time?
I can not understand the mean of these parameter at electrical characteristics, Figure 11 and Figure 13.
■At figure 11, Where is propagation delay time?
Does the propagation delay time include the dead time?
Or, is the propagation delay from the end of tDEAD_TIME to 50% rising of GHx Voltage?
■At Figure 13, Where is propagation delay time?
I thought that this tDead time is the propagation delay time because you define that tpd_Ir-O is Positive input rising to GHS_x rising at electrical characteristics.
In addition, from Figure 11, I can also think that tDead is counted from when both Gate turn off.
In conclusion, I am confused waht is propagation delay and what is dead time.
I would appreciate if you teach me the definition and how to think these.
Best regards,