Hi there,
We are having trouble with DRV8840 whose nFAULT is pulled down unexpectedly, and only way to recover DRV8840 is to reset it. We monitor the current, temperature, and VM, and none of them ever reach the protection threshold; 1A, 35 deg C, and constant 24V, respectively. Is there any other reason the DRV8840 would enter the fault state?
Thank you
regards,
Kevin