Other Parts Discussed in Thread: DRV10964
Hi Team,
Our customer is using DRV10963 in his applications. He have some questions about this device. Hoping to get your help.
- The output current of DRV10963 is 500mA according to the description of datasheet. But the Table 7 (Pg. 14) shows that ILIMIT could go up to 875mA. Could the continuous output current of DRV10963 go up to 875mA?
- The value of short circuit current protection is 1.8A when ILIMIT [2:0] = 4 (limit current is 500mA). My question is what's the value of short circuit current protection when ILIMIT [2:0] = 7 (limit current is 875mA)?
- In our product introduction page, the DRV10963 was described as "5W, 5V 3-Phase Sinusodal sensorless motor driver". Could you please explain the calculation process of this result/value 5W ?
Thanks for your help in advance.
Regards,
Ricardo Li