I'll design the bridge circuit to spin the BLDC in FOC, and I will plan to use DRV8305.
The driver needs to drive the 12 MOSFETs (each by 2 of High and low side) in total.
The Qg of MOSFET is 139nC per piece and switching frequency is 30kHz, so Gate Drive RMS Current is calculated 50mA.
Here's question. If the capacitance CPxH/L would be doubled (0.047uF -> 0.1uF) , then can DRV8305 drive 50mA?