Hi, Team
One customer reported an issue on DRV10983Z version.
When leave the SPEED PIN floating (disconnected every thing from the PIN), as spec shows, there should be a 55Kohm pull down to pull SPEED low and the motor should be stopped. But in real, there is a >1V measured on SPEED PIN and motor keeps rotating. Settings are properly loaded and SPEED is set as PWM mode.
Could you please check the SPEED PIN structure and offer an explain?
Thank you.