Hello ,
I have two questions about DRV8848:
- I see two possible idle states at xIN1 and xIN2: both low or both high, while the active state is a PWM on one of them. I tried both and it seems that my motor is running smoother and starts running at lower duty cycles with both high, avoiding a cuurent into the supply. It seems a bit unusual to me so I want to ask if it is safe for the IC.
- Is ist ok to simply connect the motor between OUT1 and OUT2 or should I better add some kind of protection circuit like a snubber RC or a TVS diode? I don't know my motors inductance but it has a short circuit current of about 5A. How to properly calculate a snubber RC circuit and how to select a TVS diode? Will a TVS withstand permanent switching?
Thanks for any help
Martin