Other Parts Discussed in Thread: LM5001
Hi,
I have designed a power supply with three phase input for my VFD, as detailed in TIDU-412A (TIDA-00173). I originally wanted an isolated 24 V supply plus a non-isolated 24V supply (sharing the same ground as PGND). The design provides an isolated 24 V supply but only provides 16V non-isolated supply (Vaux). So I have decided to use a boost switching converter to convert the non-isolated 16V to 24V. My questions are as follows:-
1) The 16V non-isolated supply (Vaux) has been derived from Vfb which is also being used as feedback to the controller. Will using Vaux, in any way disrupt the feedback being sent to the controller through Vfb?
2) Secondly, I am going to use a switching converter to boost Vax=16V to 24V. I have the attached the datasheet of the converter. Will using this converter, which is basically a high speed switching device (1.5 MHz), introduce any further complications in the overall supply design? AP3012.pdf